This ZIP file contains a Revit family for a Cooper Lighting : Fail-Safe Brand fixture, as well as supporting files that are integral to the funciton of the family in a project.


Follow these steps and Extract these files to the following locations:


Step 1. Create a Windows File Folder in the Revit Library of your choice called "Cooper Lighting".

Step 2. Create a Windows File Folder within the Cooper Lighting Folder created in Step 1 called "Fail-Safe".

Step 3. Place the un-zipped Windows product folder (e.g. "Vandal Resistant_CFL_BCBW") within the Fail-Safe Folder created in Step 2.

	(This folder contains the necessary .TXT and .CSV Type Catalog)

Step 4. Extract any <File Name>.ies files to the IES Folder, typically installed in C:\Documents and Settings\All Users\Application 	Data\Autodesk\<Revit release name>